Brief Description | |
---|---|
File: \examples\Processing\DebuggingAndTest\Scope.va |
![]() |
Default Platform: mE5-MA-VCL |
|
Short Description The Scope operator provides options for analyzing gray-scale pictures. The operator outputs a 2D waveform for each image channel by sampling input image lines. Up to four channels are supported. In a channel, each incoming line is sampled once. According to the settings you define in parameter SampleMode, the gray scale value of the first pixel in the line, the last pixel in the line, the smallest pixel value in the line, or the greatest pixel value in the line is used for sampling. |